(3)| 10/21/2017 7:37 PM | |
|
Posts: 3 Rating:
|
Hello IOT community, I was trying to install FHEM on my new IOT2040 device. The easiest way is to install a Debian OS onto IOT2040. Following this thread: https://support.industry.siemens.com/tf/ww/en/posts/debian-for-iot2000/162525/?page=0&pageSize=10 Further install FHEM https://debian.fhem.de/ and follow the manual installation procedure. Now, FHEM is working on IOT2020 / 2040 (see attached screenshot). Next I will try to prepare a YOCTO image which may can contain FHEM ? best regards Martin |
Last edited by: MartinGl at: 10/22/2017 11:08:12 AM |
|
This contribution was helpful to
|
|
| 11/17/2017 12:22 PM | |
|
Posts: 3 Rating:
|
I promised to install FHEM onto the original YOCTO Image. These were the steps I took to install FHEM succesfully onto YOCTO: - Using the current example Image V2.1.3 - open a console and preparing the network connection with iot2000setup - running following commands:
- Adding following script into the opened editor: https://github.com/hexenmeister/MyFHEM/blob/master/etc_init.d_fhem_script.txt - Further I perfomed these commands:
- I changed in fhem.cfg all entrys of "./log/" into "/opt/fhem/log" - Finally I started FHEM with that command:
See attached screenshot of the running FHEM-Server on IOT2040. The installation under YOCTO was as simple as using a Debian-Image on that device best regards Martin G. |
Last edited by: MartinGl at: 11/17/2017 12:24:03 PMLast edited by: MartinGl at: 11/17/2017 12:45:03 PM |
|
This contribution was helpful to
|
|
| 12/7/2017 8:12 PM | |
|
Posts: 37 Rating:
|
Hi MartinGl, thanks for your work! I tried the installation today and I had some issues, therefore I fixed them and made a completely automated script, see the attachment. I have done the following changes:
I didn't change the log directory to an absolute path, because the init script already changes the working folder to /opt/fhem. Just run the script as user root using the following command:
2017-12-08:I have updated the install script again, now autostart and the watchdog should work. To completely uninstall fhem, you can use these commands:
Michael Attachmentfhem_install.sh.txt (359 Downloads) |
Last edited by: turner42 at: 12/7/2017 8:41:47 PMadded comment about not working auto-start Last edited by: turner42 at: 12/8/2017 10:27:54 AMupdated script to make autostart work Last edited by: turner42 at: 12/8/2017 6:27:18 PMupdated install script, added uninstall commands Last edited by: turner42 at: 12/8/2017 6:35:39 PM |
|
This contribution was helpful to
|
|
| 3/10/2018 2:00 PM | |
|
Posts: 6 Rating:
|
I also installed fhem on the IOT2040 and added some sensors through the IO Module and the python-mraa-library.. Please find details here. |
Last edited by: iot2040ce at: 3/10/2018 2:00:56 PM |
|
This contribution was helpful to
|
|
Follow us on