Default Header
(header konnte nicht geladen werden)
(0)| 8/15/2008 12:08 PM | |
|
Posts: 1 Rating:
|
How can you send e-mail from PLC S7-224XP to a PC via GPRS modem? |
| 8/16/2008 2:42 PM | |
|
Posts: 1742 Rating:
|
Hello, May be have a look first to this: http://support.automation.siemens.com/WW/view/en/22537809 It is GPRS based, you are not sending e-mails, but the SINAUT Micro server gives you a lot of functionnality ans scalabilty. You could use WinCC flexible as OPC client. See http://support.automation.siemens.com/WW/view/en/26312201 And WinCC flexible could be sending e-mails on events: see http://support.automation.siemens.com/WW/view/en/24139712 Otherwise, Have a look to this: http://support.automation.siemens.com/WW/view/en/21692518 The router could be a MD740 which is a GPRS Router. |
Follow us on