Default Header
(header konnte nicht geladen werden)
(0)| 10/6/2008 11:31 AM | |
|
Posts: 335 Rating:
|
Can I useCPU315-2DP with siclock? What modules in which configuration do I need?Is there any example which use these two modules? |
| 10/6/2008 12:33 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello SM; This FAQ lists the various S7 CPUs that can use the NTP protocol (from Siclock, possibly) to enable time suynchronisation in a plant. They state that you can use a CPU 315-2PN/DP for that purpose. Or you can add a CP 343-1 to your configuration. http://support.automation.siemens.com/WW/view/en/17990844 And here you will find a lot of documentation on Siclock: brochures, manuals, application examples: http://www.siemens-edm.de/125.0.html?&L=2 Hope this helps, Daniel Chartier |
| 10/6/2008 5:40 PM | |
|
Posts: 1502 Rating:
|
Source-Code for DCF (Siclock) you can download here. www.oscat.de |
| 10/7/2008 9:06 AM | |
|
Posts: 335 Rating:
|
If I use CP343 with SiClock,can I connect this CP343 to WinCC (with hub or switch)for Control and Monitoring? |
Follow us on