(0)| 10/15/2008 5:17 AM | |
|
Posts: 3 Rating:
|
I have a binary tag which goes high at certain time and goes low after few minutes. I want to archieve some analog parameters during the time this bit is high. The first entryshould be at exact instance of this tag going high. The last entry should be at exact instance of this tag going low and in between that interval, there should be entries after every one minute. AttachmentNormal_setting_2.pdf (245 Downloads) |
| 10/16/2008 2:22 PM | |
|
Posts: 1776 Rating:
|
Hi, thats not possible. The delay at start and stop is causing system load, script running etc. The only possibility for exact timing is you do this at the CPU and use ARSEND see FAQ http://support.automation.siemens.com/WW/view/de/29488937 |
Follow us on