Default Header
(header konnte nicht geladen werden)
10/13/2019 10:45 PM | |
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
A direct communication between two LAN networks is not possible, see chapter "private networks" in this Link The LAN packets must be encapsulate for transmission over WAN, this is done with VPN or IP Tunnel. Because i am not an expert for WAN, VPN and IP Tunnel, search in the internet for more informations, start with the above Link. Regards, Scorp |
Follow us on