11/13/2019 7:46 AM | |
Posts: 2 Rating:
|
Dear all, greetings please your help ,I have three distributed water tanks the distance between every one and the supply pumps around 3 km so i try to make wireless communication between three slave logo_8 and the master one which near to pumps which will revive the water level signals from the three tanks ,I already made the program and the network between the four logos but during make drag drop for network input NI and network output NQ the sequential serial of NI jump direct from NI11 to NI13, NI12 not inserted and when i have try to make download to logo message came there blocks without connection to output although i removed the program and wrote again please your help thanks for all ------------------------------------------------------------------------------------------ Attachmentlogo_8.pdf (276 Downloads) |
Last edited by: Jen_Moderator at: 11/13/2019 08:43:22New subject after splitting |
|
11/13/2019 8:45 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
|
Follow us on