Default Header
(header konnte nicht geladen werden)
(0)| 11/27/2008 1:11 PM | |
|
Posts: 18 Rating:
|
hi, i am upgrading op7 with op77b. i want to download same programe of op7 in op77b. is it possible ? If yes then how &which type ofmodificationsrequired ? |
| 11/27/2008 3:38 PM | |
|
Joined: 4/24/2006 Last visit: 1/23/2026 Posts: 9107 Rating:
|
Dear Dev... You can not download OP7 programm into OP77B. Because OP7 was programmed with Protool and OP77B needs WinCC flexible. You can open protool project in WinCC flexible, the project will be migrated. See this manual: http://support.automation.siemens.com/WW/view/en/18796902 Here is also told what you should pay attention too. Best regards, Wizard |
| 12/1/2008 9:27 AM | |
|
Joined: 4/24/2006 Last visit: 1/23/2026 Posts: 9107 Rating:
|
Hi Dev... When you use WinCC flexible 2007 the migration is the same. There is no difference. Best regards, Wizard |
Follow us on