Default Header
(header konnte nicht geladen werden)
(1)| 1/9/2009 12:09 PM | |
|
Joined: 8/25/2005 Last visit: 1/14/2026 Posts: 1162 Rating:
|
Hello IC-MPE, within the german spoken forum there was a discussion which might be helpfull. Maybe you understand german? S7-300 Batteriefehler There Chris wrote that with old CPU the OB is available ( S7-300 Instruction List CPU Specifications CPUs 312 IFM to 318-2 DPS7-300) And Morten gave the information that the SFC 51 could be used. Evaluation of the LED for an S7-300 battery fault Good luck Sabine |
Follow us on