10/7/2020 12:34 AM | |
Joined: 8/27/2020 Last visit: 4/9/2025 Posts: 3 Rating:
|
Hi PoorvaGupta, I have Similar Issue going on one of the Client Machine and it's running Wincc 7.0 SP3. Wincc is Freezing in Run time and then they have to reboot the computer. Do you remember how you resolved the issue which you had few years back in wincc 6.0. It would be great help if you can share it the steps which you performed to resolve the issue. Thanks a lot in Advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/07/2020 10:29:50New subject after splitting |
|
10/7/2020 12:14 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello Avadh, if a reboot solves the problem temporarely, You should use the SIMATIC Assessment Suite - Data Collector (SAS-DC) https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Service Request, and send the diagnostic data Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on