(0)| 10/26/2020 9:33 AM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, with the provided example image you can try to install grafana and InfluxDB from source. But I am not sure if there is 32-bit sources. For Grafana, they only talking about 64-bit. Another way would be to include these programs to an image build on your own. The procedure is described here. This requires a Linux build environment. The most easy way would be to go with an IOT2050. The example image for the IOT2050 runs Debian and you can simply install the two programs via apt install. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 11/5/2020 4:04 PM | |
|
Posts: 18 Rating:
|
Thanks for answering! It looks like Influx has a 32-bit download here... https://portal.influxdata.com/downloads/ When installing this on the example image, how do I then run it ? Or get it to show up under the software in the iot2000setup menus? |
| 11/6/2020 9:22 AM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, true, haven't found that. If you download the package for ARM and extract it, you will find the binaries in the extracted folder
It won't appear in the iot2000setup tool. You can either run it manually from the mentioned folder or you create an autostart script (example see here). Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 11/6/2020 10:34 PM | |
|
Posts: 18 Rating:
|
I believe I previously downloaded the 32-bit version. There is a separate ARM version for Linux Binaries. Is this the one I want to download for the IOT2040? When I try to run the influx file within the influxdb01.3.3-1/usr/bin it says "This program can only be run on processors with MMX support." Any idea how I can work around that to get influxDB working on this? Thanks for responding |
Follow us on