1/9/2019 5:26 AM | |
Joined: 9/24/2010 Last visit: 6/12/2025 Posts: 118 Rating:
|
Hi All Pro and Friends, In 2012, Siemens presentation about SIMATIC S7-1500 &| today, this PLC generation had alot of function. So that , i make this thread, and i think we can collecting and sharing document and project about PLC S7-1500
+ PWM coding: Sample coding - Analog processsing - Redundancy or something same function. Thanks all |
Last edited by: Tranhieu0983 at: 11/22/2020 17:49:29Mechatronic Center |
|
This contribution was helpful to
1 thankful Users |
11/22/2020 5:43 PM | |
Joined: 9/24/2010 Last visit: 6/12/2025 Posts: 118 Rating:
|
I just worked with PWM functionality. Which CPU S7-1500 event Compact CPU or expansion module, you can not have Function Block or instruction to Control PWM as you want. You need to read manual with Control Interface, not too much difficult but it's not easy if you don't have any ideal about it before. Manual instruct you use WRREC, and i forget it when i have gotten some issues. But i use Control Interface and make function block easy to use. It run and i want to share this code to you: + My Project: use TIA Portal V16 + CPU: CPU 1511C, but you can use any CPU Compact S7-1500C or expansion module if you have. + Size of file : more than 12 MB so that i can not attach at here. Please go to this link: Google drive: Sample Project for PWM S7-1500 |
Mechatronic Center |
|
Follow us on