(1)| 12/8/2020 1:42 AM | |
|
Joined: 4/5/2016 Last visit: 4/21/2025 Posts: 11 Rating:
|
Hello, I have the same issue. I'm working with WinCC 7.4 SP1 Update 6. I have also a dedicated network adapter used for the redundancy. Redundancy between two servers, alarm and tag logging synchronization, are working but internal tags with "Synchronization" check won't work. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/09/2020 09:56:01New subject after splitting |
|
| 12/8/2020 8:22 AM | |
|
Posts: 7298 Rating:
|
Hello gas1993, the process "DataManager", which is responsible for the communication You could check, the eventlogs of the OS and the WinCC-Logs, You could try to install the actual Update 16 for WinCC V7.4 SP1
Georg Berghof |
Follow us on