(1)| 11/16/2020 10:57 AM | |
|
Joined: 7/16/2011 Last visit: 8/16/2024 Posts: 24 Rating:
|
Hi, I have faced the following two problems when testing the WinCC Alarm on CPU Configured alarms. 1- Some CPU Configured alarms (Alarms that sent from CPU) cannot be acknowledge when they went. I.e. the green (went alarm) keep blinking and cannot be acknowledge in any way unless I stop and start the WinCC runtime. 2- When changing main/standby CPU two alarms always remain while there should be no alarm because both CPU's and their CP are in RUN mode. Both of the above issues are indicated in the attached screenshot. The system configuration is as bellow:
I have configured and generate the the CPU reporting by "Report System Error" function in Hardware config "option" Menu. Then downloaded to PLC and compiled to WinCC. Any idea what could be the cause of this issue? Thanking you in advance for your time and help. Kind Regard ARN AttachmentAlarm_Acknowledgement_Issue_1.pdf (176 Downloads) |
Follow us on