12/16/2020 1:09 PM | |
Posts: 5 Rating:
|
Hi all, we have Wincc Runtime V7.2 + upd1 with CPU 319F. we are using SQL Server 2008R2 in production PC and we have configure the alaramlogging so that all the error is logged in Database. we have also our own scripts which runs every 10 minutes and saved the information in User Defined table. the problem we are facing from the beginning of the plant (Since 3 Year) that the alarm logging is stopped saving the Information in Database (internal Database which wincc use) and when we restart the wincc runtime that data start writing again in the database. Below is the setting of alarm logging which we have alarm logging setting (image link) i have also screenshot of database where you can see that after 12.12.2020 16.21 there is no any data and after restarting the wincc the data is appearing with the date 16.12.2020 08.25 Database image (image link) can someone guide me where is the real problem. should i have to change the setting in Alarmlogging or something else. thanks in advance for your support.
Attachmentimages.zip (225 Downloads) |
Last edited by: Jen_Moderator at: 12/17/2020 07:03:37Removed links and added files as an attachment. |
|
1/13/2021 2:45 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello Tar89, such a case needs a closer investigation. You should use the SIMATIC Assessment Suite - Data Collector (SAS-DC) https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Servicerequest and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to
1 thankful Users |
1/13/2021 2:51 PM | |
Posts: 5 Rating:
|
Hi Georg, Thank you very much for your support. I will update the post if we have find some solution to this. I really appreciate your time and effort. Regards, Tarun Patel
|
Follow us on