10/8/2006 12:15 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Muneeb, After power down and power on you might be reaching the CPU again and read out the Diagnostic Buffer. There will be given some error codes that might be pointing in the direction of the problem. It could be that a update of the firmware is possible and the DEFECTIVE status will never come again. But there fore is a diagnostic buffer and the MLFB number of your CPU 414 necessary.... [:o] The DEFECTIVE status is coming when there is no solution for something that is called, going further could be dangerous....[;)] So please place the diagnostic buffer on the forum so I could look to it. You may also look for yourself at Operating System Updates for S7-414-CPUs |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/2/2007 1:56 PM | |
Posts: 5 Rating:
|
Hi Late, Thank You for Your interest. I have attaced a document, where I hope You can see something. I have found out at least that CPU rack is NOT earthed with it's earthing point, only through power supply. Rauno Attachment414-2DP pictures.pdf (1262 Downloads) |
1/20/2007 5:50 PM | |
Posts: 5 Rating:
|
Thanks Late, There is at least an old version of firmware in CP443-1 (&GK7 443-1EX11-0XE0), which in now V2.3. Quite an old one! There is no routing used, at least not in the situation when the fault occurred. The chain of events was the following: - small changes to the existing FC blocks was downloaded, no problems - suddenly, when downloading again a small change (FDB programming, in function CMP>I, theconstant value in IN2 was changed to another constant) the fault occurred. I will open a service request to Siemens Finland. Here You can also find a zip file of installed software. Thanks, Rauno AttachmentInstalled software 20070120.zip (908 Downloads) |
Last edited by: Rane at: 1/20/2007 6:10 PM |
|
1/21/2007 3:33 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Rauno, You can update the CP 443-1EX11 and also update STEP7. CP 443 -1 Firmware Update V2.6 and Unrestricted Use in any Hardware Release (6GK7443-1EX10-0XE0 and 6GK7443-1EX11-0XE0) Service Pack 1 for STEP 7 V5.4 and STEP 7 Professional Edition 2006 If everything is up-to-date you might ask Siemens Finland with a Service Request what to do. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|