5/16/2019 2:12 PM | |
Posts: 32 Rating:
|
Hello gentlemen, ladies! I'm using TIAP V14 and am trying to connect via the ethernet cable to the LOGO 6ED1052. The LAN light on the LOGO alternates between orange and green, while the PC side shows red and flashing yellow. I've tried several cables, known to work elsewhere. I've connected the PC by opening a new project and trying to detect the unspecified CPU (as per U-TUBE video). I'm getting no response from the LOGO whatsoever. Is there perhaps something, which needs to be set ON the LOGO itself, in order to communicate? Is it at all possible, to program a LOGO with TIAP? If so, how? Any help would be greatly appreciated. Thx DBM68 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2019 14:39:38New subject after splitting |
|
5/16/2019 8:23 PM | |
Posts: 32 Rating:
|
Right.... How do I make this happen? Please also see the attachment... |
Last edited by: DBM68 at: 05/16/2019 20:27:58 |
|
5/16/2019 8:29 PM | |
Posts: 32 Rating:
|
I'm German as well.. Kannst Du so machen, bitte. |
5/16/2019 8:34 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35965 Rating:
|
Then take a look at this topic in german forum: Beispiel: Einrichten einer Kommunikation zwischen LOGO! 0BA8 und S7-1200 |
5/16/2019 8:35 PM | |
Posts: 32 Rating:
|
I will... Thank you! |
This contribution was helpful to
1 thankful Users |
5/16/2019 8:40 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35965 Rating:
|
Hello DBM68, you're welcome. If not all clear, ask. |
5/17/2019 12:07 PM | |
Posts: 32 Rating:
|
|
5/17/2019 1:28 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35965 Rating:
|
As your screenshot shows, the LOGO! is the server and the S7 is the client. Is that what you want? |