(0)| 4/20/2021 10:38 AM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello if you replace or add new modules, you have to do this in the device configuration. The firmware and the module type (article number) must match the real module. Then compile everything and download it to the CPU. Or do you want to exchange the modules during operation? In this case, you should configure the modules that support hot swapping. Which modules can you replace with S7-1500 running? With best regards |
Follow us on