(1)| 4/23/2021 2:16 PM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Please also see the attached screenshots. I need to add a new metercounter to a machine. There is already one on the machine so I want to duplicate the existing as much as possible. I am using the same FM350 module for the new counter as is used for the existing counter. I will put the counter on the same IM as the existing counter module. If I just let Simatic Manager decide it will give the module I and Q addresses 518 to 533 but the system also accepts if I type in 202 as start adresses (and the the end addresses will be 217). Will both settings work and what is most correct? So how do I put new values in the DB's?
AttachmentFC2 MT E.zip (430 Downloads) |
Follow us on