(0)| 5/2/2021 2:02 PM | |
|
Joined: 11/29/2015 Last visit: 7/3/2024 Posts: 50 Rating:
|
Hi all, I'm using the block in the link below to calculate the average of a value. https://support.industry.siemens.com/cs/ww/en/view/1021364 I have a condition for which i want the calculation of the average to start, i putted the bit condition in EN but i noticed that sometimes FB holds output status and i have to reset it manually. I've heard it's not recommended to disable block execution (EN=0) which in my case goes on and off. Could it be the reason why FB holds output status and should i put the condition bit connected in serie with the value. Thanks. |
Last edited by: horizon2015 at: 05/02/2021 14:03:00Last edited by: Jen_Moderator at: 05/03/2021 11:32:08Optimized link. |
|
Follow us on