(0)| 5/26/2021 3:43 PM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello Michal A, I can not find the SP5 for STEP 7 V5.5, only SP4. I think this is a bug by the indication so I recommend to install the hotfix 11 for STEP 7 V5.5 SP4. Use the link. Hotfix 11 download for STEP 7 V5.5 SP4 and STEP 7 Professional 2010 SR4 Use also the function "Save as" together with the option "With Reorganization (slow)" in the SIMATIC Manager. With best regardsCicero |
Follow us on