(0)| 2/18/2019 9:20 AM | |
|
Joined: 1/8/2010 Last visit: 8/18/2025 Posts: 12 Rating:
|
Hello, I have an additional question for the Proxy using. I have S7 5.5 project with S7-300 PLC where I added new TP1200 Comfort panel via TIA proxy project. It is OK, the TP1200 communicates whit PLC. But If I want to change something in PLC FB´s I not able to connect from PC to the PLC. I have to disconnect the panel from PLC. After that I can upload the change or connect to the online status. And it´s same when I want to upload a change to TP. First I have to disconnect TP from PLC. Is it standard behavior ? Or there is a mistake ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/18/2019 10:29:28 AMNew subject after splitting Last edited by: Jen_Moderator at: 2/18/2019 10:31:04 AMEdited headline. |
|
| 2/18/2019 9:25 AM | |
|
Joined: 5/12/2006 Last visit: 1/14/2026 Posts: 22800 Rating:
|
Hello, which error you get ? How the devices are wired? Christoph |
| 2/20/2019 6:12 PM | |
|
Joined: 1/8/2010 Last visit: 8/18/2025 Posts: 12 Rating:
|
For better description I add a picture - error message after unsuccessful connection to the PLC Igor |
Follow us on