Default Header
(header konnte nicht geladen werden)
(0)| 7/27/2021 4:31 AM | |
|
Joined: 1/2/2014 Last visit: 12/10/2025 Posts: 167 Rating:
|
Hello Experts, For SFC51 SSL ID 0696 and 0C96 please explain. SSL ID -->0696 INDEX -->Address with I/O ID SSL ID -->0C96 INDEX -->Start address with I/O ID What should be entered in the area of Address with I/O ID & Start address with I/O ID? ---------------------------------------------------------------------- For the below SSLID I am just sharing an informration. SSL ID -->00B1 INDEX -->Logical base address SSL ID -->00B3 INDEX -->Logical base address Logical base address = start address of IO I got the above information from this manual --------------------------------------------------------------------------- |
Last edited by: Jen_Moderator at: 07/27/2021 12:07:49Optimized link. |
|
| 7/27/2021 11:22 AM | |
|
Posts: 5521 Rating:
|
hi RIAN Che, have a look into the description of SFC51 and SZL ID. See the following manual, chapter 34.27: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 hope this helps, regards, |
This contribution was helpful to
|
|
Follow us on