Default Header
(header konnte nicht geladen werden)
(0)| 3/4/2009 10:06 PM | |
|
Posts: 1502 Rating:
|
Hi [QUOTE] Please ,is possible update gsd,konfig file,that are in HwUpdate of Step7 manager without Step7 manager ?? [/QUOTE] Yes [QUOTE] I have problem ,because notebook is not possible connected on the internetfor reasons compatibility on the my company. [/QUOTE] Do you have an CD, DVD, USB-Stick ... Yes ! Here are the HSPs. Download --> Save to a "Medium" --> Read in with Notebook --> Start --> ready http://support.automation.siemens.com/WW/view/en/23183356 |
Follow us on