(0)| 10/1/2021 2:29 PM | |
|
Posts: 1 Rating:
|
Hi, did you find the solution? I'm facing the same issue with the 6ES7534-7QE00-0AB0 Module, I tried changing the Interference suppression parameter, using Update PI instructions with Cyclic OB and nothing happened, still updates of 120 ms. it is ridiculous that being connected to the sensor in a series array to a s7-400 PLC I can get a much faster update of the signal through a variable shared by profibus communications with that PLC! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/04/2021 09:02:50New subject after splitting |
|
Follow us on