(3)| 11/25/2021 10:31 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Please also see the attached screenshots. I need to be allowed to save an FC block. I have a machine where I want to make some additions - I had made them and tried to save the FC block I got an error: "Compiler information range violation" (message 34:13). I later tried to open the block in a project right from our backup and when I try to save the block without changes I get the same error. I have tried saving my project in a new folder with reorganization - but that made no difference. How do I fix the error so I can make my changes and save the block? AttachmentEB5 Danser A.zip (388 Downloads) |
| 11/25/2021 11:35 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Hi mopS04, Thank you for answering. I don't really understand what the "Help on the message" is suggesting: "To Correct or Avoid Error: Correct the initial value you entered for the variable. In the declaration the ARRAY limits must be set so that the ARRAY has a maximum total of 65535 elements. When you edit a block via available stations or in a V2 project, an upload or copying into a V3 project can help." Can this help message be simplyfied? How do you see that the STL code has been in LAD or FCB before? Unfortunately I have read very little STL code so I am not fully aware what the STL logic is doing. Can someone translate the STL code tp "plain English"? I just tried deleting the 3 networks containing STL (1, 2 and 5 - see attached screenshots) but I still get the same error message when trying to save. Doe this mean the error is outside the STL code
AttachmentEB5 FC32 A.zip (409 Downloads) |
Last edited by: xmnj at: 11/25/2021 11:46:10Added attachment |
|
Follow us on