(0)| 10/6/2021 7:10 PM | |
|
Joined: 9/27/2006 Last visit: 12/29/2025 Posts: 12477 Rating:
|
Hello Tiger; Please tell us which version of PCS 7 you are working with, as the CPU 410-5H is only enabled with PCS 7, starting with version 8.x Normally v9 of PCS 7 should have the CPU 410-5H in its configuration files. There is no link to HSP 267 that I can locate on the forum, could you show a sceenshot of the error message you are receiving? In case this can help, there is an HUP (hardware upgrade package) for PCS 7 v8,x, an executable file that integrates the CPU 410-5H in the PCS 7 configuration: The executable will not work if you only have Step 7. https://support.industry.siemens.com/cs/ww/en/view/68627630 Hope this helps, |
| 12/10/2021 9:35 AM | |
|
Joined: 4/28/2015 Last visit: 8/11/2025 Posts: 23 Rating:
|
HSP 267 V2.0 is an internal document, please contact Siemens sales representative. |
Follow us on