(1)| 12/12/2021 8:24 AM | |
|
Joined: 4/28/2015 Last visit: 10/1/2025 Posts: 67 Rating:
|
I want to use 4 channels for counting. Wiring done. When doing the programming, I see one channel is already in use. I want to use the 2nd channel. So I inserted a network > Called SFB48 from Library > Assigned db number 61 to it and instant db created. (for earlier channel 0 the SFB48 was called using db60). Is it correct way of programming ? The parameter for SW_GATE assigned DB61.DBX 4.0 and others like this. When I download the program and go online, I see this is not executing !! Where can I be wrong ? pls see the attached online NW SW_GATE is set to 1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/13/2021 11:32:20New subject after splitting There is only one end of Knowledge, The beginning. |
|
| 12/12/2021 12:47 PM | |
|
Posts: 8092 Rating:
|
Actually I have not tried this, only 1 channel is worked out. Please refer How do you create and update multiple instances? - Siemens ... FAQ which may help you. |
Follow us on