(0)| 1/17/2022 7:13 PM | |
|
Posts: 257 Rating:
|
Hello SIOS-Forum-Community At the SIMATIC S7-300/400 under Step 7 5.x a bus diagnosis was realized with the block FB126 (formerly also FB125) and a visualization template. In the following application example this is shown on the basis of FB126 Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x) How is this implemented in the TIA Portal today and is it also available for the successor of the S7-300, the S7-1500? These are questions we are asked and the following example provides the relevant information: Diagnostics in User Program with S7-1500 More information about the integrated system diagnostics can be found in the article: System Diagnostics with S7-1500 and TIA Portal Note The procedure described in this article refers to the time of writing this article (status: January 2022). Yours sincerely SIMATIC International Technical Support Hub |
Follow us on