(0)| 1/27/2022 10:27 AM | |
|
Joined: 4/16/2013 Last visit: 4/21/2025 Posts: 5 Rating:
|
Hi I'm having difficulty using the clock pulse signal to count up accurately in my FB !! Not sure if I've missed something... but would appreciate any help before i lose my mind :) The problem is the count is incrementing way more pulses than the frequency should provide in a set period. i.e in 10 seconds using 10Hz i should have a count of 100 ? but i get a variation over 800 !! When I use the 1HZ bit there doesn't seem to be a problem ! PLC Cycle time 7ms ( range 4ms to 29ms) I have; Clock pulse bit (M0.0 -10Hz) declared as input #SpdPls #SpdPlsM = STAT #CycCnt = STAT
Any Help would be appreciated Thanks
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/27/2022 13:09:54New subject after splitting |
|
Follow us on