(4)| 4/27/2022 12:05 PM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello xmnj; Can't add much to Piscean's great reply, it is on spot. There are different ways to integrate a new gsd file in Step 7, come back to us if and when Regloplas replies to your query. One extra point: "DP-NORM" appears in your Profibus hardware configuration when you do not have the bmp files that accompany the gsd file you want to integrate in Step 7. It does not represent a specific slave model, no reason to search for it. It simply shows you did not download or properly install the icon file for your Profibus slave. Inside a standard gsd file, there is an entry "bmp_device= " where you can link the manufacturer's bmp file you dowloaded with the gsd file. That way the icon bmp for your slave will appear, instead of the annoying DP-NORM image. If you are not amused by the DP-Norm icon, you can replace it with a custom bmp, as shown in this document: https://support.industry.siemens.com/cs/bh/en/view/490268 Hope this helps, |
This contribution was helpful to
|
|
Follow us on