(2)| 11/28/2023 2:09 PM | |
|
Joined: 3/21/2013 Last visit: 8/7/2025 Posts: 24 Rating:
|
Hello, I have an issue if I used three WSTRING inputs at the CONCAT function in a FOR loop then the resulting WSTRING will have the limit around 1030-1050 characters. In other words if i use the below code then isn't works correctly (#statMeasurementsString is WSTRING[3000], #statWorkString is Array[1..50] of WSTRING)
If I split in two it works fine.
Do anybody know if is a limitation for more than two inputs ? Thanks. GabyT ------------------------------------------------------------------------------------------ |
Last edited by: GabyT at: 11/28/2023 14:27:20Last edited by: The Helping Hand at: 11/28/2023 14:28:33New subject after splitting Last edited by: GabyT at: 11/28/2023 17:55:49Last edited by: GabyT at: 11/29/2023 08:04:37 |
|
Follow us on