(0)| 1/2/2024 2:39 PM | |
|
Joined: 1/1/2024 Last visit: 3/25/2025 Posts: 2 Rating:
|
Hello to all! There is another difference between plc300 in pcs7 with TIA 1200, the program image is attached. We created station 300 in pcs7 which includes FC with Fb _DB, when we modify input block for only a block, some memory bits of fc and Fb blocks are changed together. It is very important that if someone builds these blocks and uses them, there will be interactivity that we can not find it. so may not be traceable and debugged in a large project. Issue: executing the same command in a part of the block that has no memory connection with another block. In this case, When the "Start" input of one block is modified to TRUE, the "SR" of the other block is also activated! Why? The program was simolation part of a project that is summarized in a new project. This program on another laptop by the same pcs7 has similar results. we changed it to static type (for Fb) but the interaction between memories was yet. But it works properly in Tia portal.. Why are those really related? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/03/2024 10:57:11New subject after splitting |
|
Follow us on