Default Header
(header konnte nicht geladen werden)
(0)| 1/6/2024 11:17 AM | |
|
Posts: 3 Rating:
|
Hello Friends I tried to practice with the use of FileWrite but I was only able to create the file as you can see in the attachments. I could not load data into the file. For example, I tried to load an integer 3 into the file using the FileWrite Block from the PLC program but the file created is only showing a character. I could not see the number "3" . I am trying to understand the use of the FileWrite block so that after I can use the FileRead easily. Thanks Abiodun ------------------------------------------------------------------------------------------ AttachmentFileWrite_issues.zip (199 Downloads) |
Last edited by: Jen_Moderator at: 01/08/2024 11:17:52New subject after splitting |
|
| 1/8/2024 11:18 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to use of FileRead and FileWrite is published within the conference STEP 7 (TIA Portal). Jen_Moderator |
Follow us on