1/17/2024 10:28 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi hewking103, If what you want is to start the clients, you must "Interconnect" the servers project from SIMATIC Shell, not launch the mcx directly. You may also find the following FAQ helpful in configuring clients: "What settings do you have to make when installing a multiple station system in SIMATIC WinCC Professional?" I hope this information can be of help to you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on