(0)| 1/27/2023 1:18 PM | |
|
Joined: 2/20/2014 Last visit: 12/16/2025 Posts: 405 Rating:
|
Hi I managed to to do a complete uninstallation for TIA Portal V13 using the Inventory Tool. But I did not managed to do the same for TIA Portal. V15 & V17. Only the file type "SEPRO" was removed but the file type "SEPA" all remained. I had then attempted to uninstall via the Control Panel > Program & Features then followed by Settings > APPS (both also failed). I had then attempted to do the uninstallation using the DVD but also failed (there was this message "Initialization of the product has failed" & "Couldn't initialize no products"). Please help to provide the solution on how I can completely uninstall the TIA Portal V15 & V17. AttachmentTIA Portal V15 & V17 uninstallation error.zip (751 Downloads) |
| 1/26/2024 11:18 AM | |
|
Joined: 2/27/2021 Last visit: 5/15/2025 Posts: 12 Rating:
|
Any solution? It happens the same to me with v17 |
Follow us on