(0)| 2/16/2024 5:48 PM | |
|
Joined: 4/20/2021 Last visit: 11/12/2025 Posts: 3 Rating:
|
How do i do vbscript in Wincc screen? Im fairly new at this however i intend to do the same. I want the plc to read data on HMI tags. Basically i have 8 s7-1200 1215 cpus in daisy chain arrangement linked to the HMI (HMI connected with first plc) I want all of the PLC'S to read the HMI tags data. Since it is easier on hmi screen to put data and make plc read them I have tried put get commands and modbus tcp for sharing data to a single plc and then reading from it but its invain had a hard time trying to get to read it but i feel this is easier
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/19/2024 09:28:52New subject after splitting |
|
| 2/22/2024 9:19 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello ABD.HAS00 its not 100% clear whats your usecase. If you just want to connect a S71200 to an HMI for reading/writing tags then you can do this: https://support.industry.siemens.com/cs/de/en/view/89852595 if you want to share data between the PLCs with HMi then this would be the wrong way of doing. The HMi Is not made for sharing Data between different PLCs. You should make the PLC/PLC communication instead. But it would be great if you could give us a few more information about your devices and Usercases Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on