(1)| 2/21/2024 8:24 AM | |
|
Joined: 5/6/2022 Last visit: 11/27/2025 Posts: 589 Rating:
|
If I have not checked correctly, you still need to install the version of WinCC RT Advanced V17 so that you can run the simulation of a Comfort screen. As you can see in the release note it seems to indicate that it is necessary to simulate: "Delivery Release SIMATIC WinCC V19" I would recommend installing it and checking if the simulation already allows it. Here are some download links if they are useful: "SIMATIC WinCC V17 Runtime (TIA Portal)" "Updates for WinCC Runtime Advanced V17" I hope I was able to help you! Best regards! |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 2/21/2024 4:43 PM | |
|
Joined: 11/16/2022 Last visit: 10/8/2025 Posts: 6 Rating:
|
Thanks, it's exactly the solution. I've install WinCC Runtime Advanced V17 and now, i can start the simulation for comfort panel in Tia Portal V19. Problem solved. Have a nice day, |
This contribution was helpful to
|
|
Follow us on