(0)| 12/1/2020 4:18 PM | |
|
Posts: 3 Rating:
|
Good evening, I use Windows 7 and TIA Portal v14 SP1. When I look in the "Online access" folder after starting the TIA Portal, there are only COM and TeleService adapters and PN/IE adapters are missing. I can ping the PLC without any problems. I noticed in the Service Manager that I do not have the "SIMATIC PnDiscovery Service" running. When I try to start this service (C: \ Program Files \ Common Files \ Siemens \ Automation \ Simatic OAM \ bin \ s7oPNDiscoveryx64.exe), nothing happens. I reinstalled TIA Portal several times, but without any change. On the second computer, where there is also Windows 7 and the same version of TIA Portal v14 SP1, everything goes smoothly. Has anyone encountered this problem? Thank you for all the advice. ms ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2020 09:03:40New subject after splitting |
|
| 3/14/2024 2:43 PM | |
|
Joined: 11/27/2023 Last visit: 10/1/2025 Posts: 3 Rating:
|
I dont see this service running in my Services list, is there a way to install it? |
Follow us on