(0)| 3/27/2024 1:59 AM | |
|
Posts: 2 Rating:
|
How do you set the Max Cycle Time into 250ms?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/27/2024 06:50:26New subject after splitting |
|
| 3/27/2024 8:31 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi,
before spending time in the wrong direction: Which TIA version is used? Because with the latest updates for V16 and V17 this message can be unchecked that it shall not be displayed anymore. Why do you get one of the following messages: "The cycle time may increase (0601:000044)" or "Possible cycle time violation (0601:000042)"?Remedy With TIA Portal V16 Update 6, TIA Portal V17 Update 4 and TIA Portal V18, the following change has been implemented: When monitoring is switched on, a dialog box warns of the possible increase in the cycle time. In this dialog box, you can continue or abort the monitoring. To prevent this dialog box from being displayed again, while the project is open, check the check box "Do not show again" and end the dialog with "Yes". regards sancruz |
|
Feedback appreciated, please rate |
|
This contribution was helpful to
|
|
Follow us on