(0)| 2/13/2024 3:22 PM | |
|
Joined: 5/3/2021 Last visit: 12/19/2025 Posts: 63 Rating:
|
Hello Denilson, We have been using TIA 17 with the 'traditional' access control. We use this for secure communication between the HMI (WinCC comfort panels V2) and the PLC (1517F). Now we are switching to TIA 19 with WinCC Unified panels. After I downloaded the new PLC (1517F FW3.1) and the nice new Unified panels, there is no communication (even not when I disable access control). Only when I activate the Legacy and fill in the passwords like normal, than it works normally. However, I guess the plan is to step away from the old legacy stuff and use the newer access control philosophy. But what passwords and where do we need to configure this? Is there a manual available? With Kind regards, Colin van den Mosselaar ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/14/2024 09:01:53New subject after splitting Yes to all |
|
Follow us on