(0)| 10/11/2021 10:07 PM | |
|
Joined: 10/16/2020 Last visit: 10/10/2025 Posts: 3 Rating:
|
Anyone have the issue where TIA admin says there are updates available, but none of the program tabs under Software Management show any type of update available? On mine the icons next to the search for update, both show zero updates, if I scroll through each program and check each Tab there is nothing to download or install. When I ran TIA updater last week and found several updates, but they would not show up in the TIA Admin, even after downloading and installing them. However I did notice If I restart my computer then open TIA administrator, it will show that the Language packages I previously installed, need installed again. I have License manager and software updater running when I try to use TIA Admin. Other things I have tried: Running Updater and License Mang. as an admin. Double checked my Internet Options. Ran TIA Admin on Chrome, Edge, and Firefox (my default is chrome) Turned off all browser securities. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2021 09:01:14New subject after splitting Last edited by: cwykeae at: 10/12/2021 20:17:07 |
|
| 11/11/2022 3:29 PM | |
|
Posts: 1 Rating:
|
I have the same problem. Has anyone found a solution? |
Follow us on