(0)| 8/29/2024 6:25 AM | |
|
Joined: 7/10/2024 Last visit: 1/13/2026 Posts: 180 Rating:
|
Hello! A Step 7 Basic license is sufficient for the task you are looking for, as these are used to program the 1200 PLCs. If you have a CPU 1500 it would have to be the Professional version. Then you need a WinCC Basic license to program the basic panel. Here is the link so you can see all the information related to TIA 18. Sales and Delivery Release of Tia Portal V18 (Anyway, I remember that if you open a Support Request telling your case, they tell you directly the MLFB you need). |
|
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
| 8/29/2024 6:31 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Hi, When you want to use S7-1200 and HMI Basic panel, you can use the following software: Step 7 Basic v19: 6ES7822-0AA23-0YA5 (for configuration of SIMATIC S7-1200; SIMATIC Basic Panels; SIMATIC Unified Basic Panels;) Best regards, Wizard |
This contribution was helpful to
|
|
Follow us on