(0)| 3/18/2019 6:49 PM | |
|
Joined: 6/12/2016 Last visit: 9/13/2025 Posts: 3 Rating:
|
I'm trying to load a program into a hmi ktp 700, but I can not. I can ping, online acess , too At first because I could not establish communication, I loaded a program by usb. I configured the ip by the start center. But now i can't load a program by usb because in the start center the "setting" and "transfer" are disable only "start" is enable, see the attached file. Now is imposible to download a program to this hmi. I tried to reset by usb but it doesn't work What I can do it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/19/2019 6:52:49 AMNew subject after splitting |
|
| 3/23/2019 6:55 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello Armando Fiestas, What is the firmware version of the HMI panel? Also see the possibility to find out HMI panel details using SIMATIC Automation Tool Hope you used USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels for reset to factory settings. Use the firmware >= V14.0.1.4
|
Last edited by: Jen_Moderator at: 3/25/2019 11:40:46 AMOptimized links. Like it? Rate it! |
|
| 10/4/2024 12:26 PM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello aligenc If you have a Basic Panel 2nd Generation then you cannot use Prosave to do a Reset to factory settings. This will work only with the USB Recovery: https://support.industry.siemens.com/cs/ww/en/view/109744950 What does not work with that? If you have trouble check a few other USB Memory devices. It has to be USB 2.0 and not so big, I only have also 1-2 USB sticks that works for the USB recovery. For me some older 2.0 2GB sticks works well Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on