2/12/2024 10:33 AM | |
Joined: 1/3/2018 Last visit: 7/18/2025 Posts: 33 Rating:
|
Good morning, we are facing the same problem, in one project we have defined two F-CPU S71500 and we exchange standard and safety telegrams. Data in standard telegrams are good, but we get errors in hw configuration due to safety telegrams. Especially one CPU has only the bit SUBS_ON high without errors, instead the other CPU has SUBS_ON high and diagnostic errors RET_DPRD = 16#80A0 and RET_DPWR = 16#80A1. Checking in the overview of addresses we do not see any overlapping of addresses both in tag tables, program info and hw configuration looking into the network properties. DP_DP_ID are configured accordingly (twisted in SENDDP and RCVDP). The weird thing is that the same configuration is working in same project but related to two different CPUs in a different network. Do you have any ideas? Installed software: Attachmentimg.zip (292 Downloads) |
Last edited by: Corn98 at: 02/12/2024 10:59:48 |
|
1/9/2025 4:09 PM | |
Joined: 6/5/2023 Last visit: 7/3/2025 Posts: 1 Rating:
|
Corn 98 did you solve it? I have the same problem |
Follow us on