1/30/2025 6:24 PM | |
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
OK, here is SCL FB which works, but there is a problem I can't resolve. 3 positions are set by one pushbutton correctly, but I want it to reset to OFF position when simulation is finished, or PLC's power supply fail . The problem is that it remembers the last state it was before I stopped the simulation. Can you fix it to work as expected, please? AttachmentSCL.txt (156 Downloads) |
1/31/2025 9:08 AM | |
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
OK, here is archive with video, SCL and TIA V19 3-way position switch. You don't have to spent 2 days dealing with it, as I did. The only flaw of this program is that switch and the rest of the faceplate don't show-up and disappear synchronously, there could be a small time lag, but it is not important. The problem was how to control facaplate and its switch visibility at the same time with FB output and HMI tags. Don't mind the rest of the program, it is unfinished ATS switch. AttachmentATS 3-1 02.02.2025.zip (137 Downloads) |
Last edited by: milos23 at: 02/02/2025 14:26:30 |
|
Follow us on