(0)| 2/3/2025 9:27 AM | |
|
Joined: 7/10/2024 Last visit: 1/13/2026 Posts: 180 Rating:
|
Hello IvanNaperz! Based on what you say, I recommend you check the following FAQ, where you can check the requirements to have a parallel installation of different versions. https://support.industry.siemens.com/cs/ww/en/view/109827320 Also, it would be interesting to know if this happens in a single project that you have been migrating, or if you create a new basic project it also happens. Finally, I recommend you check that the operating system is compatible with the software you have installed on the computers. I leave you the Compatibility tool. I hope this comments are helpful. |
|
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
| 2/3/2025 12:12 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi IvanNaperz, In this case, the problem is that the operating system version you have (OS: Windows 11 Home 24H2) is not compatible with any version of TIA Portal. The 'Home' OS versions are not recommended to be installed together with Siemens software as it does not have the requirements to run these programs. The behavior is non-compatible or untested operating systems may or may not work as the environment is not released and it is not really known how it will work as it may give unexpected errors. I attach the Windows 11 compatibility Excel so you can check it. In this case, I recommend you to use a released operating system to ensure compatibility with Siemens software. If not, you may have problems like the one you are experiencing. Best regards!
AttachmentMicrosoft-Windows-11_es_2025-02-03.xlsx (302 Downloads) |
|
If this Information really helps, you could use the Rate function |
|
| 2/20/2025 7:49 PM | |
|
Joined: 11/24/2019 Last visit: 12/4/2025 Posts: 2 Rating:
|
i have the same problem, my windows version is Windows 11 Pro 24H2 |
| 2/21/2025 8:12 AM | |
|
Joined: 7/10/2024 Last visit: 1/13/2026 Posts: 180 Rating:
|
Hello! AsElonksuM_SN_BN said, it is possible that it is due to the 24h2 version of Windows, since Siemens has not yet made any compatibility report on TIA Portal. Apart from this, I would review the questions in my previous post in this thread, and if the problem is general, I would recommend a repair/reinstallation of TIA Portal, always doing this with the software installer itself. The latter is very important (which is very important).
|
|
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
Follow us on