3/3/2025 4:57 PM | |
Joined: 3/3/2025 Last visit: 3/3/2025 Posts: 1 Rating:
|
I am running into the same issue here. I've followed to clear temp data, and also tried to run the installation from cmd. But it returned "Installation Failed" without no further info. I am in Windows 10.0.19045. Installing V4.0 was fine. Although, after restart, the app didn't open and gave a crash .dmp file. Then when installing V4.0 SP1, installation throw the same error AutoGen experienced. Installing V6.0 worked well and the app opens as normal. But unfortunately I can't use this version to connect to Process Simulate. So v4.0 is the only way forward. Is there anything I can check and debug? TIA
------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_1128023 at: 03/03/2025 17:39:15Last edited by: Moderator_Lan at: 03/04/2025 09:30:53New subject after splitting Last edited by: Moderator_Lan at: 03/04/2025 09:32:07Citation added |
|
Follow us on