3/17/2025 6:17 AM | |
Joined: 2/27/2025 Last visit: 3/17/2025 Posts: 1 Rating:
|
I'm facing a problem with Desigo CC-V7.0 BACnet alarm configuration in PXC-100 controller. When I am configuring "Standard Alarm" in Desigo CC for any parameter with Delay time, it's working in both side. For example, If I give Delay time for 120 Seconds, when that value goes out of range then it waits for 120 seconds to create an alarm and when again comes in normal range it takes again 120 seconds to become normal. But I need instant normal condition, no need to wait again 120 seconds to show normal. On the other hand, Those alarms are not smooth enough, like the alarm remain active even after value becomes normal. what can I do now to solve this issue? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/17/2025 10:05:13New subject after splitting |
|
Follow us on