(0)| 7/1/2025 1:29 PM | |
|
Joined: 10/25/2019 Last visit: 9/10/2025 Posts: 3 Rating:
|
Ayman Elotaify in Problem to get access in the SIMATIC panel: In any case, if you can't access any passworded object, there will be the following reasons for that:
To do it:
Hope this helps. Can I also do this procedure for HMI panels that are running TIA? I have a KTP600 basic mono PN with image V11 (TIA11 I guess). I have just uploaded complete backup using Prosave. Since I don't have TIA11 I was thinking to create a new project with user administration in TIA14 (or never, which I have). And then make backup image of the user management. However I have doubts that this will work because full backup will be from V11 and user management backup from V14. Will this work? Othervise I'll need to get TIA11 to have same image versions I guess… Thank you so much!
------------------------------------------------------------------------------------------ |
Last edited by: nlamgo at: 07/01/2025 13:29:40Last edited by: Moderator_Lan at: 07/01/2025 13:56:13New subject after splitting Last edited by: nlamgo at: 07/02/2025 07:08:25to add a context which was lost because ob thread split |
|
Follow us on