9/15/2025 12:41 PM | |
Joined: 1/17/2024 Last visit: 9/18/2025 Posts: 18 Rating:
|
Hello, I am working with TIA Portal V20 and using a CPU 1517H-3 PN (6ES7 517-3HP00-0AB0). The hardware has been connected, and the network architecture is configured correctly in TIA Portal. When I run the project with WinCC RT Advanced V20 (PC Station), the communication works fine and I can see the output as expected. A video is attached below showing the test and the issue. Has anyone faced a similar issue?
Any guidance or suggestions would be very helpful. Thanks in advance, AttachmentScreen Recording 2025-09-15 174318.mov (4 Downloads) |
Follow us on